CW V10.6 debug problem occurred

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW V10.6 debug problem occurred

1,944 Views
nietongnie
Contributor II

CW V10.6 debug problem occured ,the chip is MC56F84789.

Labels (1)
1 Reply

1,874 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

first, we need to know the problem is in one specific project or a common issue for all projects?

if you create a new project with wizard and new workspace, can you download the program to the board?

if not, please let me know:

1. do you use MC56F84789 demo board or self-desinged board? if demo board, what interface do you use? on board osjtag or external usb tap?

2. check your windows device manager, can it recognize the interface well?


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply