I wrote a program about GPIO used codewarrior10.6 for MC56F84789. When I download the program,i can't download other program for MC56F84789.but MC56F84789 is runing.,  I wrote a program about GPIO used codewarrior10.6 for MC56F84789. When I download the

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I wrote a program about GPIO used codewarrior10.6 for MC56F84789. When I download the program,i can't download other program for MC56F84789.but MC56F84789 is runing.,  I wrote a program about GPIO used codewarrior10.6 for MC56F84789. When I download the

1,072件の閲覧回数
xinzhujiang
Contributor I

when i download other program ti's ok.but when i download the GPIO's program,i can't download other program.

ラベル(1)
0 件の賞賛
返信
1 返信

988件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

MC56F84789 uses jtag  for on chip emulation and download.

while for MC56F84789, some jtag pin is multiplexed with GPIO. see datasheet, page 17,18.

http://www.nxp.com/files/dsp/doc/data_sheet/MC56F844XX.pdf?fasp=1&WT_TYPE=Data%20Sheets&WT_VENDOR=FR... 

if you defile the related jtag pin as GPIO, the jtag feature can not work  normal.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信