CW_11, S08QG, How can I save a project and develop it further withou to create a new projekt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW_11, S08QG, How can I save a project and develop it further withou to create a new projekt

Jump to solution
2,514 Views
Mei
Contributor IV

Hallo dear community,

If a project is saved with his name and I want to develop it further or start a new one, I only know one way to do this: I have to load a project example from CW and modify it. What's a better way, similar to WORD with "save as" and writing go on?

.With best regards

Gerd Meinert 

 

 

0 Kudos
Reply
1 Solution
2,502 Views
Mei
Contributor IV

Dear Jun Zhang,

Thank you for your answer.

 You got me right. I went your way:  - New - Bareboard Project - Name - MC9S08QG8 - p & E USB MultiLink -Relocatable Assembly -without Processor Expert - Finish .... project is created.

The head is not the same as in my project based on the CodeWarrior example project, but I will be able to work with it.

Thank you!

 

View solution in original post

0 Kudos
Reply
2 Replies
2,503 Views
Mei
Contributor IV

Dear Jun Zhang,

Thank you for your answer.

 You got me right. I went your way:  - New - Bareboard Project - Name - MC9S08QG8 - p & E USB MultiLink -Relocatable Assembly -without Processor Expert - Finish .... project is created.

The head is not the same as in my project based on the CodeWarrior example project, but I will be able to work with it.

Thank you!

 

0 Kudos
Reply
2,507 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

Not sure if I understand your question. If you want to start a new project, go to below to create a new one.

ZhangJennie_0-1603700577831.pngZhangJennie_0-1603700577831.png

 

If you want to continue working on your existing project, just open it with IDE then you can go on working with it.

If this doesn't answer, please be more specific on your question. I will check it further.

 

Have a nice day,

Jun Zhang

 

 

 

0 Kudos
Reply