CW 10 debugger mouse hover

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CW 10 debugger mouse hover

1,811件の閲覧回数
wba
Contributor III


In CW10 debugger, if I hover the mouse over a variable it shows the value.  How can I change the display format (ie a char variable to  show the hex value instead of the ascii char)?

ラベル(1)
0 件の賞賛
返信
1 返信

1,644件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Bruce:

I think that is not possible. The format for the hover is always Decimal or ASCII in this case. You can change the display format but only for the Variables view (at upper right corner). Check the next tutorials that might be useful for you:

Hovering and Debugging | MCU on Eclipse

Debugging Variables in Hexadecimal with Eclipse | MCU on Eclipse


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信