CW 10: Controlling Link Order

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CW 10: Controlling Link Order

1,630件の閲覧回数
dougpaulsen
Contributor IV

Is there any way to control the link order in CodeWarrior 10.4 for HCS08 micros?  There's buzz about a "Link Order tab" but that seems to be limited to ARM, et al.  The only way I can control the link order is to disable "Generate Makefiles automatically" in project->properties->C/C++Build then manually shuffle the file list in the <project>.args file.  Seems like there ought to be a more simple way ('cause I'll forget I've disabled makefile generation and have all sorts of contortions later on).

Thanks for any pointers!

タグ(1)
0 件の賞賛
返信
1 返信

1,581件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Doug,

There is no option in CW10.4 for HCS08 to change link order 

Your method is the exact method to do it. 


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信