CW 10: Controlling Link Order

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW 10: Controlling Link Order

1,542 Views
dougpaulsen
Contributor IV

Is there any way to control the link order in CodeWarrior 10.4 for HCS08 micros?  There's buzz about a "Link Order tab" but that seems to be limited to ARM, et al.  The only way I can control the link order is to disable "Generate Makefiles automatically" in project->properties->C/C++Build then manually shuffle the file list in the <project>.args file.  Seems like there ought to be a more simple way ('cause I'll forget I've disabled makefile generation and have all sorts of contortions later on).

Thanks for any pointers!

0 Kudos
Reply
1 Reply

1,493 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Doug,

There is no option in CW10.4 for HCS08 to change link order 

Your method is the exact method to do it. 


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply