CF Flasher windows 8

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

CF Flasher windows 8

跳至解决方案
3,303 次查看
kappa74
Contributor IV

Good morning,
I have a question about flash programmer for Coldfire.

Up to now I use the CF Flasher with Windows XP.

But now I have a new PC with Windows 8.1 and the CF Flasher doesn't work because it can't initialize the BDM device which is the PE Multilink Universal.

Is there a version of the CF Flasher for Windows 8.1?

Or is there an alternative flash programmer for Coldfire (MCF52255) which runs in Windows 8.1 for the PE Multilink Universal?

 

Thank you

Best Regards

标签 (1)
0 项奖励
回复
1 解答
2,544 次查看
TICS_Fiona
NXP Employee
NXP Employee

Hello Mirko

Unfortunately the CFFlasher does not support Windows 8.1. It only works on Windows XP or 2000.

You can use the Flash Programmer in CodeWarrior v10.6.4.  CW10.6.4 can be downloaded from:

http://tinyurl.com/6jo5tge

To program Coldfire in CW10.6.4 IDE, you may create a Target Task for flash programmer, or use the 'Flash File to Target' feature.

For details, please view the section <Debugger->Flash Programmer> in v10.x FAQ Guide:

C:\Freescale\CW MCU v10.6.4\MCU\Help\PDF\Microcontrollers_FAQ_Guide.pdf

To use it as a standalone tool, please see below for how to do it:

http://mcuoneclipse.com/2012/08/02/standalone-flash-programmer/

Here is CodeWarrior Flash Programming from a DOS Shell

http://mcuoneclipse.com/2012/08/03/codewarrior-flash-programming-from-a-dos-shell/

Best Regards

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,545 次查看
TICS_Fiona
NXP Employee
NXP Employee

Hello Mirko

Unfortunately the CFFlasher does not support Windows 8.1. It only works on Windows XP or 2000.

You can use the Flash Programmer in CodeWarrior v10.6.4.  CW10.6.4 can be downloaded from:

http://tinyurl.com/6jo5tge

To program Coldfire in CW10.6.4 IDE, you may create a Target Task for flash programmer, or use the 'Flash File to Target' feature.

For details, please view the section <Debugger->Flash Programmer> in v10.x FAQ Guide:

C:\Freescale\CW MCU v10.6.4\MCU\Help\PDF\Microcontrollers_FAQ_Guide.pdf

To use it as a standalone tool, please see below for how to do it:

http://mcuoneclipse.com/2012/08/02/standalone-flash-programmer/

Here is CodeWarrior Flash Programming from a DOS Shell

http://mcuoneclipse.com/2012/08/03/codewarrior-flash-programming-from-a-dos-shell/

Best Regards

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复