Bin files for nor flash for faeries and p series processors

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Bin files for nor flash for faeries and p series processors

1,147件の閲覧回数
monalihaware
Contributor III

Where can I find bin files for p series and t series of qoriq processor viz p2020 and t2080

タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,084件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Monali Haware,

Please download QorIQ Linux SDK 1.9 prebuilt image ISO QorIQ SDK V1.9 PPCE500V2 IMAGE ISO from Previous version link from Linux® SDK for QorIQ® Processors|NXP, please use u-boot image in p2020rdb folder.

For T2080, please download SDK 2.0 prebuilt image ISO QorIQ Linux SDK v2.0 PPCE6500 IMAGE from Latest Version link from Linux® SDK for QorIQ® Processors|NXP, please use u-boot image in T2080RDB folder.

In addition, for custom boards bringing up, you could download and install CodeWarrior for PA 10.5.1 from CodeWarrior Development Studio for Processors|NXP, then create a bareboard project, build and running the elf on the target board, you could select the SRAM launch configuration when create the bareboard project to avoid configuring DDR controller.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,084件の閲覧回数
monalihaware
Contributor III

Hello Yiping,


1. I downloaded and extrated the iso file. But it shows .bin files sizes as 0kB. snapshot attached.

2. Any application note for each of this extracted file? iso.PNG

0 件の賞賛
返信