CodeWarrior command line interface for download

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior command line interface for download

Jump to solution
3,000 Views
hyunuk_ha
Contributor I

Dear ZhangJennie‌, 

I succeedded compile my project using your article as attached. 

But is there any way to,

1. Automated download way( using command line interface), or

2. Download command line interface(Attached document includes compile process only)

Please help me with an urgent and important issue.

My project is PIL(Processor In the Loop) simulation based on simulink platform.

Thank you in advance.

Regards,

Hyunuk

# codewarrior‌ , commandlineinterface‌

Labels (1)
1 Solution
2,877 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Hyunuk,

Professor Erich Styger ever wrote article about CodeWarrior Flash Programming from a DOS Shell.

CodeWarrior Flash Programming from a DOS Shell | MCU on Eclipse 

Please check if this can help you.


Have a great day,
Jun Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
2,877 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Hyunuk,

Professor Erich Styger ever wrote article about CodeWarrior Flash Programming from a DOS Shell.

CodeWarrior Flash Programming from a DOS Shell | MCU on Eclipse 

Please check if this can help you.


Have a great day,
Jun Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------