Bared project using gcc and c++  , debug failed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Bared project using gcc and c++  , debug failed

1,394件の閲覧回数
matherinewang
Contributor III

Hello,

I create a new bared project, which using gcc and c++.

I build the project sucessful, then debug but failed as show below.

It' a empty project so i think it will not exceeded the size limit, but why failed?

 

14395_14395.pngpastedImage_0.png

ラベル(1)
0 件の賞賛
返信
1 返信

1,302件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello matherine wang:

Is this the Special edition CodeWarrior for MCUs?

If so, then it does not support C++ code, only C. The next article will explain you this error window:

Please Check Your License | MCU on Eclipse


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信