Automotive Math and Motor Control Library Set for NXP  MPC560xP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Automotive Math and Motor Control Library Set for NXP  MPC560xP

1,918件の閲覧回数
hqin
Contributor I

Dear Sir or Madam, 

 

I am a design engineer working for De Amertek Co. I am interested in the  library of 'Automotive Math and Motor Control Library Set for NXP  MPC560xP'. I download a evaluation license from your web. But it doesn't  include the peripherals blocks like ADC, PWM, CAN etc. Can I get a  evaluation license of that library including the peripherals blocks for MATLAB? Is there any demo models which can be provided?

 

Sincerely,  

Hao

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,603件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello Qin

Automotive Math and Motor Control Library supplies the mathematical library, general functions for digital filter and motor control. It does not include the driver for peripheral modules.

User can get the examples for ADC, PWM, CAN etc of MPC560xP from the our website www.nxp.com by searing “AN2865”. Hope it helps!

Best Regards

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信