Ask: codewarrior(V10.6) how to run the script file that makes oneself?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ask: codewarrior(V10.6) how to run the script file that makes oneself?

Jump to solution
1,912 Views
liangrunzhou
Contributor I

Ask: codewarrior(V10.6) how to run the script file that makes oneself

0 Kudos
Reply
1 Solution
1,804 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Zhou,

I suggest you refer this article

CodeWarrior 10 Command Line Interface – usage and examples 

You can include the command on command prompt into the script file and run them to make the project itself.


Have a great day,
Jun Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,805 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Zhou,

I suggest you refer this article

CodeWarrior 10 Command Line Interface – usage and examples 

You can include the command on command prompt into the script file and run them to make the project itself.


Have a great day,
Jun Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply