Ask: codewarrior(V10.6) how to run the script file that makes oneself?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Ask: codewarrior(V10.6) how to run the script file that makes oneself?

ソリューションへジャンプ
1,934件の閲覧回数
liangrunzhou
Contributor I

Ask: codewarrior(V10.6) how to run the script file that makes oneself

0 件の賞賛
返信
1 解決策
1,826件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Zhou,

I suggest you refer this article

CodeWarrior 10 Command Line Interface – usage and examples 

You can include the command on command prompt into the script file and run them to make the project itself.


Have a great day,
Jun Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,827件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Zhou,

I suggest you refer this article

CodeWarrior 10 Command Line Interface – usage and examples 

You can include the command on command prompt into the script file and run them to make the project itself.


Have a great day,
Jun Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信