ARM Flash Programmer Task

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ARM Flash Programmer Task

2,928 Views
lizboxy
Contributor I

Sir:

Use LS1020 and  Codewarrior V11.4.4  on WIN10.

But can not add flash in ARM Flash Programmer Task in attached, due to not connect the EVK board?

Also try to use OCRAM,but still in Grey which can not be accessed.

Any adviseTks!

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

2,870 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please open CodeWarrior IDE with the following command in the shell console.

C:\Freescale\CW_ARMv7_v2019.10\CW_ARMv7\eclipse\cwide.exe -nl en

0 Kudos
Reply