ARM Flash Programmer Task

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ARM Flash Programmer Task

2,932件の閲覧回数
lizboxy
Contributor I

Sir:

Use LS1020 and  Codewarrior V11.4.4  on WIN10.

But can not add flash in ARM Flash Programmer Task in attached, due to not connect the EVK board?

Also try to use OCRAM,but still in Grey which can not be accessed.

Any adviseTks!

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

2,874件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please open CodeWarrior IDE with the following command in the shell console.

C:\Freescale\CW_ARMv7_v2019.10\CW_ARMv7\eclipse\cwide.exe -nl en

0 件の賞賛
返信