支持ColdFire V4e core内核,可以直接创建纯汇编工程模板的软件开发工具推荐

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

支持ColdFire V4e core内核,可以直接创建纯汇编工程模板的软件开发工具推荐

Jump to solution
1,074 Views
GAO123
Contributor III

基于MCF5474VR266单片机开发,需要可以创建纯汇编工程模板的软件开发工具,请推荐。

0 Kudos
Reply
1 Solution
1,041 Views
GAO123
Contributor III
感谢您的回复,我想再问下,Codewarrior v11.1 版本针对MCF5474VR266型号的单片机可以直接创建汇编软件模板工程吗?而不是通过C工程内联调用汇编。

View solution in original post

0 Kudos
Reply
12 Replies
1,058 Views
Celeste_Liu
NXP Employee
NXP Employee

Hello @GAO123 ,

请参考CodeWarrior Development Suites | NXP Semiconductors ,可以看到下面两个是支持ColdFire V4的:

Codewarrior v11.1:

Celeste_Liu_0-1750392297099.png

Codewarrior v7.2:

Celeste_Liu_1-1750392309899.png

希望能帮到你。

BRs,

Celeste

 

---------------------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!
---------------------------------------------------------------------------------------------------------------------------------

 

0 Kudos
Reply
1,042 Views
GAO123
Contributor III
感谢您的回复,我想再问下,Codewarrior v11.1 版本针对MCF5474VR266型号的单片机可以直接创建汇编软件模板工程吗?而不是通过C工程内联调用汇编。
0 Kudos
Reply
1,026 Views
Celeste_Liu
NXP Employee
NXP Employee

应该是可以的。在新建项目时Language那一项选择“ASM"。

Celeste_Liu_0-1750648291711.png

 

0 Kudos
Reply
1,022 Views
GAO123
Contributor III
麻烦您选择 ColdFire V4e core,型号为 MCF5474测试下,是否有ASM语言选项,我这边是没有的。另外bin文件能导入工程吗?
0 Kudos
Reply
1,004 Views
Celeste_Liu
NXP Employee
NXP Employee

有安装coldfire的插件吗?

Celeste_Liu_0-1750659888838.png

点击Help->Install New Software:

Celeste_Liu_1-1750660035155.png

 

0 Kudos
Reply
1,001 Views
GAO123
Contributor III
您这边安装新的插件,选择ColdFire V4e core和MCF5474VR266型号,是会出现ASM语言的选项?
0 Kudos
Reply
997 Views
Celeste_Liu
NXP Employee
NXP Employee

我这边还没有试,因为一些原因我这边codewarrior v11.1需要重新安装。如果需要的话我等会安装成功了帮您试一下。

0 Kudos
Reply
995 Views
GAO123
Contributor III
感谢,感谢,麻烦您帮我试下。
0 Kudos
Reply
982 Views
Celeste_Liu
NXP Employee
NXP Employee

Hello @GAO123 ,

试了一下,确实没有“ASM”。

Celeste_Liu_0-1750678534820.png

 

0 Kudos
Reply
968 Views
GAO123
Contributor III
有没有办法直接创建汇编工程模板呢?
0 Kudos
Reply
968 Views
GAO123
Contributor III
收到!谢谢。另外,可以导入bin文件,进行仿真、调试模式?
0 Kudos
Reply
1,023 Views
GAO123
Contributor III
您选择 ColdFire V4e core,型号为 MCF5474VR266,可以吗?我这边在这个型号下没有语言选择项
0 Kudos
Reply