外部RAM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

外部RAM

1,075 Views
wuming
Contributor I

S12XEP100如何使用外部RAM  ex. page RAM_F0 ,RAM_F1 ?

Labels (1)
0 Kudos
Reply
1 Reply

1,025 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

HI

S12XE expanded bus has the similar functionality and features to S12XD devices, so you can refer to following ANotes. Useful links regarding S12X ext bus design: http://www.freescale.com/files/microcontrollers/doc/app_note/AN2708.pdf

In An2992 there is an example of interfacing with a device connected to expanded bus.

http://www.freescale.com/files/microcontrollers/doc/app_note/AN2992.pdf


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------