License file

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

License file

1,767 Views
evanlim
Contributor I

Hi,

 

I'm using MobileGT V9.2 software with CodeWarrior USB TAP (cwh-ctp-base-he) on a window XP laptop.

 

I'm able to perform flash programming and hardware diagnostic testing when using the original license file.

However, after I use the license file that I had generated for that window XP laptop, I'm unable to perform both flash and hardware testing.

 

May I know what's wrong with the license file that I had generated?

154010_154010.pngpastedImage_0.png

Thanks!

 

Regards,

Evan

Labels (1)
0 Kudos
Reply
2 Replies

1,698 Views
TICS_Fiona
NXP Employee
NXP Employee

Hello Evan

For the license issue, I would suggest submitting a case. It's better under case process for private license details. For how to submit a case, please refer to:

https://community.freescale.com/docs/DOC-330215

Best Regards

Fiona Kuang

TIC - Technical Information Center

0 Kudos
Reply

1,698 Views
evanlim
Contributor I

Hi Fiona,

I had already submitted the case twice since end of June and I have yet to receive any reply from NXP.

I need the license file urgently as the 30days license file had already expired.

Thanks.

Regards

0 Kudos
Reply