useing RTRT with Codewarrior

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

useing RTRT with Codewarrior

2,376 Views
metro
Contributor I
hello,
 
I am trying to use RTRT with Codewarrior for C++. Is there any special flag settings needed in this case. Can i use the same C flags for C++ also?
 
Hope you can give some insight.
 
 


Message Edited by CrasyCat on 2007-09-24 09:04 AM
Labels (1)
0 Kudos
Reply
1 Reply

1,153 Views
CrasyCat
Specialist III
Hello
 
I am not sure what RTRT is?
What are you trying to do here?
 
- Which CPU are you targeting (HC08, HC12, Coldfire, ..)
- Which version of CodeWarrior are you using?
  To retrieve that info:
    - Start CodeWarrior
    - Select Help -> About Freescale CodeWarrior
    - Click on "Install Products"
    - CodeWarrior version used is displayed on top in the Installed Products dialog.
 
CrasyCat
0 Kudos
Reply