tool chain error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,082件の閲覧回数
ankurchauhan
Contributor I

I'm trying to import exiting .mcp project file (demo project given by freescale).

its giving the "this tool chain is not supported for this target" error.

what could be the issue???

print-screen of error is bellow:

 

 

 

81724_81724.pngpastedImage_1.png

 

Regards

Ankur

ラベル(1)
0 件の賞賛
返信
1 解決策
2,808件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Ankur,

I don't have practice with this TWR-LCD module but most of the time a CD or other quick manual is delivered inside the package.

According to the web info the Kit Contains

  • TWR-LCD module
  • Necessary cables
  • DVD with demo projects, software, training and collateral
  • Quick Start Guide document

Most of examples are based on Processor Expert.

I recommend to have a look to the link:

          Graphical LCD Tower System Module|Freescale

The examples could be dedicated to a processor.

The advantage of Processor Expert is you can change the processor.

Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
2,807件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi,

This feature is supporting DSC project only.

For other devices, you can not use it.

Application note to import classic project under Eclipse

There are 2 ANs explaining the process depending of the architecture used.

        AN4727, Import project from CW classic to CW MCU v10 4 CodeWarrior for Microcontrollers v10.4

                        http://cache.freescale.com/files/soft_dev_tools/doc/app_note/AN4727.pdf

        AN4104, Converting ColdFire Projects to CodeWarrior Development Studio for Microcontrollers V10.0

                        http://cache.freescale.com/files/soft_dev_tools/doc/app_note/AN4104.pdf

hope this will help


Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,807件の閲覧回数
ankurchauhan
Contributor I

Hi pascal

What all software's are required to configure twr-lcd (without LCDC controller).

I'm using bareboard project without processor-expert and trying to use LCD via flexbus  but its not working.

can you help me in this ,i want to display some alapha-numeric characters on screen.

Regards and thanks

Ankur

0 件の賞賛
返信
2,809件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Ankur,

I don't have practice with this TWR-LCD module but most of the time a CD or other quick manual is delivered inside the package.

According to the web info the Kit Contains

  • TWR-LCD module
  • Necessary cables
  • DVD with demo projects, software, training and collateral
  • Quick Start Guide document

Most of examples are based on Processor Expert.

I recommend to have a look to the link:

          Graphical LCD Tower System Module|Freescale

The examples could be dedicated to a processor.

The advantage of Processor Expert is you can change the processor.

Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,807件の閲覧回数
ankurchauhan
Contributor I

Hi Pascal,

Can you tell me how to import the demo project in to my workspace.

Regards and Thanks

Ankur

0 件の賞賛
返信
2,807件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi Ankur,

Sorry for the delay I was in vacation last week.

You can import a project in a workspace via the  menu:

    File + Import...

          General + Existing Projects Into Workspace

              you can select the project you want and recommend to select the option" Copy projects into workspace" to have all files under your workspace.

Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信