some problems about  CW 8.8 when I make the  programme

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

some problems about  CW 8.8 when I make the  programme

ソリューションへジャンプ
2,794件の閲覧回数
Freshman
Contributor III

hello :

     I writed a programme,

 

#include <stdio.h>

#include <stdlib.h>

int main(int argc , char **argv )

{

  printf("Hello World !");

}

 

 

but when I make it,there comes 10 errors as the follow:

 

Link Error : undefined :'__init_hardware'

Referenced from '__start' in Runtime.PPCEABI.H.UC.a

、、、

Link failed.

 

help,who can tell me what is wrong?

 

thank you.

bin

ラベル(1)
0 件の賞賛
返信
1 解決策
2,580件の閲覧回数
CrasyCat
Specialist III

Regarding the issue with File error 206009, did you check following post in the forum?

CW 8.8 file error 206009 when creating new project for P1020RDB

Regarding the linker issue, did you create your project using the wizard?

Is there a file __ppc_eabi_init.c in your project? This is where the function __init_hardware is implemented.

CrasyCat

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
2,580件の閲覧回数
Freshman
Contributor III

hi

     When I creat a project in CW8.8 ,  I meet the problem as the follows:

111.jpg

who can help me ? and I just do as the user manual !

0 件の賞賛
返信
2,580件の閲覧回数
CrasyCat
Specialist III

Hello

Which OS are you running on your Host system (Windows XP, Windows 7, ...)?

CrasyCat

0 件の賞賛
返信
2,580件の閲覧回数
Freshman
Contributor III

hi catherine

My host system is Windows XP

bin

0 件の賞賛
返信
2,581件の閲覧回数
CrasyCat
Specialist III

Regarding the issue with File error 206009, did you check following post in the forum?

CW 8.8 file error 206009 when creating new project for P1020RDB

Regarding the linker issue, did you create your project using the wizard?

Is there a file __ppc_eabi_init.c in your project? This is where the function __init_hardware is implemented.

CrasyCat

0 件の賞賛
返信
2,580件の閲覧回数
Freshman
Contributor III

tahnk you very much @CrasyCat , i am too careless to see the fomer answers.

bin

0 件の賞賛
返信