need information

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

need information

1,285件の閲覧回数
anandask
Contributor I

hello all,

 

i want know what is the exactly differnce b/w mpc565 and mpc5566 processor ...

 

thanks..

ananda sk

ラベル(1)
0 件の賞賛
返信
1 返信

1,128件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

MPC565 and MPC5566 are two different products.

Below is the detailed information for these two targets:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MPC565

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MPC5566

MPC565 is usually used in industry control , and it has e500 core inside.

MPC5566 is usually used in automotive application, and it has e200 core inside.

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信