how to use code warrior for programming a mc68hc908bd48

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to use code warrior for programming a mc68hc908bd48

3,784件の閲覧回数
quimey
Contributor I
hola i´m new in the subjet.i need knowledge as using code warrior 6 for burn the program to the  mc68hc908bd48, and if somebody knows how is  the connections using the serie port or the usb port.
please hel me.bye
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,665件の閲覧回数
J2MEJediMaster
Specialist I
It's not clear to me what you're trying to do. You want to burn the program into Flash, but what is your debugger connection to the hardware? Are you trying to develop code, or just take an existing S-record file and load it into Flash?

---Tom

0 件の賞賛
返信

1,665件の閲覧回数
Vhugo9
Contributor I

Hi, any help, i am using code warriors and MPC8560, I just want to take an existing srec file into flash? how to do it... sorry i am new on this matter..

0 件の賞賛
返信

1,665件の閲覧回数
J2MEJediMaster
Specialist I

You should start a new thread when asking a question that uses a different processor.

 

Having said that, let me now try to answer your question. I am looking at the the CodeWarrior for Power Architecture 8.8 documentation. In the IDE User's Guide (CodeWarrior IDE 5.7 Windows's User Guide.pdf), Chapter 22, there is information on the flash programmer window. As its name suggests, you use this window to program the flash. On page 268, which describes the Prgram Verify panel, there is an option, File Type. This option lets you select the type of file you use as the data source for the programming operation. One of the supported choices is S-record. Consult the manual for more detail on how to set up this window for programming operations.

 

---Tom

0 件の賞賛
返信