USB TAP - ONCE for MC56F8346 using 56800E Flash programmer sw.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB TAP - ONCE for MC56F8346 using 56800E Flash programmer sw.

2,885 Views
NanosecPeter
Contributor I

Hi,

 

I have small production run of 50 boards. I was successfully programmed 46 of them using the USB TAP Once, but 4 failed to program. Here is the error message:

 

>>Connected to local CCS server at PORT 41475
>>Configured to use CodeWarrior USB TAP
>>Placing the device into debug mode, please wait...
>>CCCSClient::ResetToDebug: Network timeout

 

What can be wrong?

Thanks,

Peter

Labels (1)
0 Kudos
Reply
1 Reply

1,180 Views
barbara_johnson
NXP Employee
NXP Employee

Hi Peter,

 

This is the StarCore for DSPs forum. Please post your question to this forum.

CodeWarrior for 56xxx DSC

0 Kudos
Reply