how to use code warrior for programming a mc68hc908bd48

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to use code warrior for programming a mc68hc908bd48

3,887 Views
quimey
Contributor I
hola i´m new in the subjet.i need knowledge as using code warrior 6 for burn the program to the  mc68hc908bd48, and if somebody knows how is  the connections using the serie port or the usb port.
please hel me.bye
Labels (1)
0 Kudos
Reply
3 Replies

1,768 Views
J2MEJediMaster
Specialist I
It's not clear to me what you're trying to do. You want to burn the program into Flash, but what is your debugger connection to the hardware? Are you trying to develop code, or just take an existing S-record file and load it into Flash?

---Tom

0 Kudos
Reply

1,768 Views
Vhugo9
Contributor I

Hi, any help, i am using code warriors and MPC8560, I just want to take an existing srec file into flash? how to do it... sorry i am new on this matter..

0 Kudos
Reply

1,768 Views
J2MEJediMaster
Specialist I

You should start a new thread when asking a question that uses a different processor.

 

Having said that, let me now try to answer your question. I am looking at the the CodeWarrior for Power Architecture 8.8 documentation. In the IDE User's Guide (CodeWarrior IDE 5.7 Windows's User Guide.pdf), Chapter 22, there is information on the flash programmer window. As its name suggests, you use this window to program the flash. On page 268, which describes the Prgram Verify panel, there is an option, File Type. This option lets you select the type of file you use as the data source for the programming operation. One of the supported choices is S-record. Consult the manual for more detail on how to set up this window for programming operations.

 

---Tom

0 Kudos
Reply