If you still meet some problem about your connection.
Some customer meets a problem similar to your issue due to the voltage of the Parallel port.
See below details:
Customer engineers examined the parallel port and found that the voltage supplied to the wiggler through the parallel port was about 1v. At least 3v must be supplied to the wiggler for proper operation.
Several users meet the same problem.
Can you please check it on your side ?
See below some tips fixing XP problems.
> (A) In windows XP/2000, the parallel port dialog checkbox entitled
> "Enable Legacy Plug and Play" should be checked. This setting is located
> in the Control Panel-->System-->Hardware->Device Manager->Ports->Printer
> Port (LPTX) dialog.
>
> (B) Here are the steps to modify the parallel port registry key
> appropriately:
>
> 1. save the winxp1.reg file to your hard drive
> 2. make sure you are logged in as the system administrator
> 3. run the winxp1.reg file (by double clicking on it)
> 4. A question will be displayed "Are you sure you want to add the
> information in c:\winxp1.reg to the registry?"
> 5. Click the Yes button
> 6. A message will display "Information in c:\winxp1.reg has been
> successfully entered into the registry."
> 7. restart your computer to apply the new changes
Try the following steps in the CCS Console window:
1. ‘show wdv’ à"WinDriver V5.05b Jungo (c)2002 Build Date: Aug 4 2002 X86 SYS"
2. Start à Settings à Control Panel à System à Hardware à Device Manager
Ports à Printer Port(LPT1) double click on this and on the window go to the Resources tab.
Look at the I/O Range. The first I/O range is the address of the parallel port.
3. delete all
config cc parallel:0x0378
After doing this you should connect to the board without any problems.
This error was appearing when a customer would try to connect to the debugger.
Pascal