error-demonstration version.too many source line records.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

error-demonstration version.too many source line records.

3,005件の閲覧回数
biter
Contributor I

I am using codewarrior for MCP55xx/56xx V2.10. And i debugged a project and connected into the MCU(MPC5644A) like picture 1.

143533_143533.png搜狗截图16年03月08日1036_1.png

At last this error appeared like picture 2.

 

143486_143486.png搜狗截图16年03月07日2052_1.png

It seem i can only download 5000 line source line records.

If i want to load more source line into the MCU,what should i do.

thank you very much.

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,495件の閲覧回数
384753860
Contributor I

你好刘峰,我想请问一下你的这个问题解决了吗?我也遇到同样的问题了,能不能加微信(15398019254也是电话)交流一下。我们项目上在用5644A,以后可以多多交流。

0 件の賞賛
返信

2,495件の閲覧回数
zeyulu
Contributor I

Hi,

   I just meet the exactly the same program error.

   The problem is that I don't quite understand the answer,particularly how to "add an additional key for Win32_Plugins_Link_PPC",where is this "Win32_Plugins_Link_PPC" is and how to "add an additional key"?

   Can any one give me more specific  procedure to solve this question?(I am using the company's computer and change the licence is not an option for now)

   thanks very much!

0 件の賞賛
返信

2,495件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi,

You're using MPC55xx/56xx V2.10.

There is a Debugger issue with MPC55xx/56xx V2.10 too similar to CW for HC12 V5.1

Officially the USBDongle is not working on Win7 for Classic IDE.

We recommend to rehost the license file to Disk/Host ID.

Now if it's not an option we can propose you a workaround:

    add an additional key for Win32_Plugins_Link_PPC

Please log the request to our case system.

To submit your case into the new system, please follow below steps:

  1) Go to http://www.nxp.com/support/sales-and-support:SUPPORTHOME.

  2) On the bottom of the page under Submit New Issues, click Hardware & Software.

  3) Register with your business email to access NXP technical online support.

  4) A verification email will be sent to your account. Click the link embedded in that email to verify your access.

  5) On the NXP online support page, select Contact Support from the top menu and click “submit a new case” to start the process.

Regards

Have a great day,
Pascal
NXP Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信