downloading the program occurs error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

downloading the program occurs error

Jump to solution
2,394 Views
guofeng
Contributor II

Hi,

    How to deal with the problem, al following:

1.png2.png3.png

the device is MM912F634

Best regard!

Guofeng Lai

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
2,081 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Guofeng

If use 32bit xp,from first screenshot, your chip is secured.

On the debugger go to the menu TBDML HCS12->Unsecure...

 

This will run the "TBDML_Erase_unsecure_hcs12xx.cmd" file.

please check if your chip can be successfully unsecured.

if Unsecure can not fix the problem, try create a brand new project, test if the new project can be downloaded.

If still can't connect board, please test your board with another interface to verify if the chip itself has problem.

 


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
3 Replies
2,081 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi guofeng

I noticed you use TBDML interface. Did you work with it on 64bit win7 platform?

Please notice TBDML is not supported on 64bit platform with CodeWarrior.

Most of our customers use BDM multilink interface on 64bit windows.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,081 Views
guofeng
Contributor II

Hi Jennie,

   Thank you for your response.

   The project is built on 32bits XP platform. and I have downloaded the program successfully before. Is there something wrong in the IC?

Best regard!

Guofeng Lai

0 Kudos
Reply
2,082 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Guofeng

If use 32bit xp,from first screenshot, your chip is secured.

On the debugger go to the menu TBDML HCS12->Unsecure...

 

This will run the "TBDML_Erase_unsecure_hcs12xx.cmd" file.

please check if your chip can be successfully unsecured.

if Unsecure can not fix the problem, try create a brand new project, test if the new project can be downloaded.

If still can't connect board, please test your board with another interface to verify if the chip itself has problem.

 


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply