downloading the program occurs error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

downloading the program occurs error

ソリューションへジャンプ
2,465件の閲覧回数
guofeng
Contributor II

Hi,

    How to deal with the problem, al following:

1.png2.png3.png

the device is MM912F634

Best regard!

Guofeng Lai

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,152件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Guofeng

If use 32bit xp,from first screenshot, your chip is secured.

On the debugger go to the menu TBDML HCS12->Unsecure...

 

This will run the "TBDML_Erase_unsecure_hcs12xx.cmd" file.

please check if your chip can be successfully unsecured.

if Unsecure can not fix the problem, try create a brand new project, test if the new project can be downloaded.

If still can't connect board, please test your board with another interface to verify if the chip itself has problem.

 


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,152件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi guofeng

I noticed you use TBDML interface. Did you work with it on 64bit win7 platform?

Please notice TBDML is not supported on 64bit platform with CodeWarrior.

Most of our customers use BDM multilink interface on 64bit windows.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,152件の閲覧回数
guofeng
Contributor II

Hi Jennie,

   Thank you for your response.

   The project is built on 32bits XP platform. and I have downloaded the program successfully before. Is there something wrong in the IC?

Best regard!

Guofeng Lai

0 件の賞賛
返信
2,153件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Guofeng

If use 32bit xp,from first screenshot, your chip is secured.

On the debugger go to the menu TBDML HCS12->Unsecure...

 

This will run the "TBDML_Erase_unsecure_hcs12xx.cmd" file.

please check if your chip can be successfully unsecured.

if Unsecure can not fix the problem, try create a brand new project, test if the new project can be downloaded.

If still can't connect board, please test your board with another interface to verify if the chip itself has problem.

 


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信