compiling error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

compiling error

4,440件の閲覧回数
pallav
Contributor I
if i get my code size >1024 byte it give tthat it is more then 1024 so cant compile plz help me where to set i have initialy set the model tiny is this a prob plz help me how to resolve this prob
 
best reards
pallav aggarwal
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,061件の閲覧回数
Andrew
Contributor I

Hi,

it is probably a license error: CW doesn't find the file "license.dat". Are you working in a Remote Desktop Connection with XP? In this case CW search the license in a wrong directory!

Bye

 

0 件の賞賛
返信

2,061件の閲覧回数
BlackNight
NXP Employee
NXP Employee
Hi,
another hint is that you check your license settings. For this simply launch the compiler in the prog directory (e.g. chc12.exe for the HC12 compiler), and then check the diagnostics in the about box (Help > About).

Erich
0 件の賞賛
返信

2,061件の閲覧回数
CrasyCat
Specialist III

Hello

which processor are you targeting (HC08, HC12, ...)?

Which version of CodeWarrior are you using? To get that info:
  - Start IDE
  - Select Help -> "About Metrowerks CodeWarrior"
  - Click on "Installed Products" button.

Version you are using is indicated on the top part of the dialog.

CrasyCat

0 件の賞賛
返信