compiling error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

compiling error

4,450 次查看
pallav
Contributor I
if i get my code size >1024 byte it give tthat it is more then 1024 so cant compile plz help me where to set i have initialy set the model tiny is this a prob plz help me how to resolve this prob
 
best reards
pallav aggarwal
标签 (1)
0 项奖励
回复
3 回复数

2,071 次查看
Andrew
Contributor I

Hi,

it is probably a license error: CW doesn't find the file "license.dat". Are you working in a Remote Desktop Connection with XP? In this case CW search the license in a wrong directory!

Bye

 

0 项奖励
回复

2,071 次查看
BlackNight
NXP Employee
NXP Employee
Hi,
another hint is that you check your license settings. For this simply launch the compiler in the prog directory (e.g. chc12.exe for the HC12 compiler), and then check the diagnostics in the about box (Help > About).

Erich
0 项奖励
回复

2,071 次查看
CrasyCat
Specialist III

Hello

which processor are you targeting (HC08, HC12, ...)?

Which version of CodeWarrior are you using? To get that info:
  - Start IDE
  - Select Help -> "About Metrowerks CodeWarrior"
  - Click on "Installed Products" button.

Version you are using is indicated on the top part of the dialog.

CrasyCat

0 项奖励
回复