ccs_config_chain: error39; failed to correctly configure jteg chain.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ccs_config_chain: error39; failed to correctly configure jteg chain.

1,201 Views
set
Contributor I

hi,

 i am using cw for my own board having mpc8313e-revc. its showing following errors. ccs protocol plugin: failed to correctly configure the jteg chain;

plz tell me what could be the possible reasons for the error.

 

error log is as follows:

 

CCS: 0000    :    ccs_open
CCS:        :        ipaddr = 127.0.0.1
CCS:        :        port = 41475
CCS:        :        timeout = 10
CCS:        :        serverh = 0
CCS:        :    ccs_open; ccs_error = 0
CCS: 0000    :    ccs_get_connection_count
CCS:        :        serverh = 0
CCS:        :        count = 1
CCS:        :    ccs_get_connection_count; ccs_error = 0
CCS: 0000    :    ccs_available_connections
CCS:        :        serverh = 0
CCS:        :        count = 1
CCS:        :    ccs_available_connections; ccs_error = 0
CCS: 0000    :    ccs_available_connections
CCS:        :        serverh = 0
CCS:        :        count = 1
CCS:        :    ccs_available_connections; ccs_error = 0
CCS: 0000    :    ccs_available_connections
CCS:        :        serverh = 0
CCS:        :        count = 1
CCS:        :    ccs_available_connections; ccs_error = 0
CCS: 0000    :    ccs_available_connections
CCS:        :        serverh = 0
CCS:        :        count = 1
CCS:        :    ccs_available_connections; ccs_error = 0
CCS: 0000    :    ccs_set_timeout
CCS:        :        serverh = 0
CCS:        :        timeout = 10
CCS:        :    ccs_set_timeout; ccs_error = 0
CCS: 0000    :    ccs_config_server
CCS:        :        serverh = 0
CCS:        :        cc = 0
CCS:        :        server_config = 0
CCS:        :        value = 4030
CCS:        :    ccs_config_server; ccs_error = 0
CCS: 0000    :    ccs_get_config_chain
CCS:        :        serverh = 0
CCS:        :        device_list: (size = 0)
CCS:        :    ccs_get_config_chain; ccs_error = 0
CCS: 0000    :    ccs_config_chain
CCS:        :        serverh = 0
CCS:        :        cc = 0
CCS:        :        device_list: (size = 1)
CCS:        :            device[0]:: core_type=55;    device_descr=[ir_length:0;dr_bypass_length:0;bypass_instruction:0]
CCS:        :    ccs_config_chain; ccs_error = 39
CCS:        :        Error message:
mpc83xx: Core not responding

CCS: 0000    :    ccs_close
CCS:        :        serverh = 0
CCS:        :    ccs_close; ccs_error = 0

Labels (1)
0 Kudos
Reply
1 Reply

924 Views
set
Contributor I

i had checked following reasons:

power at pin 6

 updated cw patch for 8.7 or 8.8

reinstall and run setup.bat

 

on the  warrior connection server; it shows following

 

(bin) 5 % config load
There are no command converters configured
Server listening on port: 41475
Default configuration file loaded

0 Kudos
Reply