When trying to open the project using CW 8.5 , following error is encounetred "CodeWarrior encountered an unhandled exception 0xe06d7363 at address 0x759cc54f. Location: KERNELBASE.dll:0x759cc54f

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

When trying to open the project using CW 8.5 , following error is encounetred "CodeWarrior encountered an unhandled exception 0xe06d7363 at address 0x759cc54f. Location: KERNELBASE.dll:0x759cc54f

2,745 次查看
neelimapasupule
Contributor I

When trying to open the project using CW 8.5 , following error is encounetred "CodeWarrior encountered an unhandled exception 0xe06d7363 at address 0x759cc54f. Location: KERNELBASE.dll:0x759cc54f.

 

Can you please help resolving this issue.

标签 (1)
2 回复数

2,430 次查看
TomasPaez
NXP Employee
NXP Employee

Try to run with compatibility mode,

Run the app with right click and choose compatibility mode for the app.

2,430 次查看
neelimapasupule
Contributor I

Hi Tomas,

When I ran CW 8.5 in compatibility mode it worked fine. Thank you for your input.

BR,

Neelima

0 项奖励
回复