When trying to open the project using CW 8.5 , following error is encounetred "CodeWarrior encountered an unhandled exception 0xe06d7363 at address 0x759cc54f. Location: KERNELBASE.dll:0x759cc54f

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

When trying to open the project using CW 8.5 , following error is encounetred "CodeWarrior encountered an unhandled exception 0xe06d7363 at address 0x759cc54f. Location: KERNELBASE.dll:0x759cc54f

2,756件の閲覧回数
neelimapasupule
Contributor I

When trying to open the project using CW 8.5 , following error is encounetred "CodeWarrior encountered an unhandled exception 0xe06d7363 at address 0x759cc54f. Location: KERNELBASE.dll:0x759cc54f.

 

Can you please help resolving this issue.

ラベル(1)
2 返答(返信)

2,441件の閲覧回数
TomasPaez
NXP Employee
NXP Employee

Try to run with compatibility mode,

Run the app with right click and choose compatibility mode for the app.

2,441件の閲覧回数
neelimapasupule
Contributor I

Hi Tomas,

When I ran CW 8.5 in compatibility mode it worked fine. Thank you for your input.

BR,

Neelima

0 件の賞賛
返信