Unable to download Codewarrior for coldfire 5.1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to download Codewarrior for coldfire 5.1

Jump to solution
2,115 Views
ivansteinberg
Contributor I

I want to debug and then migrate my old M68331 project to modern MCF5xxx, but found that codewarrior for coldfire version 6 and 7 do not supports m68331, it supports only coldfire v2 MCU.

Old 3.2 version uses obsolette debuggers (parallel and serial from PE micro) and there are no way to apply patches from PE that enable modern USB

I`m unable to find any download link for codewarrior for coldfire 5.1

Is anybody can share installer?

I saved my old license file, but lost installer

1 Solution
1,785 Views
stanish
NXP Employee
NXP Employee

Ivan,

There is currently an issue with out transfer service.

I've alternatively put the installer here: 

CW_ColdFire_5.1.2_Update.zip - Google Drive 

Regards,

Stan

 

 

View solution in original post

3 Replies
1,785 Views
ivansteinberg
Contributor I

Hello, Stanislav.

Still not received any download link.

0 Kudos
Reply
1,786 Views
stanish
NXP Employee
NXP Employee

Ivan,

There is currently an issue with out transfer service.

I've alternatively put the installer here: 

CW_ColdFire_5.1.2_Update.zip - Google Drive 

Regards,

Stan

 

 

1,785 Views
stanish
NXP Employee
NXP Employee

Hello Ivan,

I've just transcended the CW for CF v5.1 + Update v5.1.2 installer to you.

You should get an notification email including download link soon.

Please let me know if you have any problem to download it.

Hope that helps.

Stan

0 Kudos
Reply