Unable to download Codewarrior for coldfire 5.1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to download Codewarrior for coldfire 5.1

ソリューションへジャンプ
2,134件の閲覧回数
ivansteinberg
Contributor I

I want to debug and then migrate my old M68331 project to modern MCF5xxx, but found that codewarrior for coldfire version 6 and 7 do not supports m68331, it supports only coldfire v2 MCU.

Old 3.2 version uses obsolette debuggers (parallel and serial from PE micro) and there are no way to apply patches from PE that enable modern USB

I`m unable to find any download link for codewarrior for coldfire 5.1

Is anybody can share installer?

I saved my old license file, but lost installer

1 解決策
1,804件の閲覧回数
stanish
NXP Employee
NXP Employee

Ivan,

There is currently an issue with out transfer service.

I've alternatively put the installer here: 

CW_ColdFire_5.1.2_Update.zip - Google Drive 

Regards,

Stan

 

 

元の投稿で解決策を見る

3 返答(返信)
1,804件の閲覧回数
ivansteinberg
Contributor I

Hello, Stanislav.

Still not received any download link.

0 件の賞賛
返信
1,805件の閲覧回数
stanish
NXP Employee
NXP Employee

Ivan,

There is currently an issue with out transfer service.

I've alternatively put the installer here: 

CW_ColdFire_5.1.2_Update.zip - Google Drive 

Regards,

Stan

 

 

1,804件の閲覧回数
stanish
NXP Employee
NXP Employee

Hello Ivan,

I've just transcended the CW for CF v5.1 + Update v5.1.2 installer to you.

You should get an notification email including download link soon.

Please let me know if you have any problem to download it.

Hope that helps.

Stan

0 件の賞賛
返信