Unable to add files

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Unable to add files

跳至解决方案
2,338 次查看
giacomopetrini
Contributor IV

Hello,

I'm using CW8.3 for 56F800/E on Win7.

All worked well until last week, when I fried my laptop... To solve (fast) the problem I got a new laptop and put the old HD (so no reinstall). Of course Win was not very happy nad since the PC is used by another person that doesn't like the default language (italian) I decided to upgrade tu Win7 Ultimate.

 

Problem is (that I discovered just now) I cannot add files to any project (new and old) anymore. If I drag the files CW remains silent. If I right click on the file list and choose "Add files", if I add a .h CW remain silent, if I add a .c CW tells me that "At leastone file could not be added to selected targets".

 

Any idead where I can begin to look?

 

Thanks Bye Giacomo

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
2,200 次查看
giacomopetrini
Contributor IV

Ok, problem solved. I was trying to add a file with the same name of one already in the project...doh.

Bye Giacomo

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,201 次查看
giacomopetrini
Contributor IV

Ok, problem solved. I was trying to add a file with the same name of one already in the project...doh.

Bye Giacomo

0 项奖励
回复
2,200 次查看
CrasyCat
Specialist III

Hello

If you switched to a new Host PC, the single node license you were using till now will not work anymore on the new PC.

You need to rehost your license.

Go to www.Freescale.com then click on My Freescale. Log in into Freescale space and click on CodeWarrior Licensing.

From there you should be able to rehost your license.

CrasyCat

0 项奖励
回复
2,200 次查看
giacomopetrini
Contributor IV

I'm using the special version, so no license needed.

But the problem was another (see my other post).

Thank you anyway.

Bye Giacomo

0 项奖励
回复