Unable to add files

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,303件の閲覧回数
giacomopetrini
Contributor IV

Hello,

I'm using CW8.3 for 56F800/E on Win7.

All worked well until last week, when I fried my laptop... To solve (fast) the problem I got a new laptop and put the old HD (so no reinstall). Of course Win was not very happy nad since the PC is used by another person that doesn't like the default language (italian) I decided to upgrade tu Win7 Ultimate.

 

Problem is (that I discovered just now) I cannot add files to any project (new and old) anymore. If I drag the files CW remains silent. If I right click on the file list and choose "Add files", if I add a .h CW remain silent, if I add a .c CW tells me that "At leastone file could not be added to selected targets".

 

Any idead where I can begin to look?

 

Thanks Bye Giacomo

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
2,165件の閲覧回数
giacomopetrini
Contributor IV

Ok, problem solved. I was trying to add a file with the same name of one already in the project...doh.

Bye Giacomo

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,166件の閲覧回数
giacomopetrini
Contributor IV

Ok, problem solved. I was trying to add a file with the same name of one already in the project...doh.

Bye Giacomo

0 件の賞賛
返信
2,165件の閲覧回数
CrasyCat
Specialist III

Hello

If you switched to a new Host PC, the single node license you were using till now will not work anymore on the new PC.

You need to rehost your license.

Go to www.Freescale.com then click on My Freescale. Log in into Freescale space and click on CodeWarrior Licensing.

From there you should be able to rehost your license.

CrasyCat

0 件の賞賛
返信
2,165件の閲覧回数
giacomopetrini
Contributor IV

I'm using the special version, so no license needed.

But the problem was another (see my other post).

Thank you anyway.

Bye Giacomo

0 件の賞賛
返信