Unable to add files

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to add files

Jump to solution
1,343 Views
giacomopetrini
Contributor IV

Hello,

I'm using CW8.3 for 56F800/E on Win7.

All worked well until last week, when I fried my laptop... To solve (fast) the problem I got a new laptop and put the old HD (so no reinstall). Of course Win was not very happy nad since the PC is used by another person that doesn't like the default language (italian) I decided to upgrade tu Win7 Ultimate.

 

Problem is (that I discovered just now) I cannot add files to any project (new and old) anymore. If I drag the files CW remains silent. If I right click on the file list and choose "Add files", if I add a .h CW remain silent, if I add a .c CW tells me that "At leastone file could not be added to selected targets".

 

Any idead where I can begin to look?

 

Thanks Bye Giacomo

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
1,205 Views
giacomopetrini
Contributor IV

Ok, problem solved. I was trying to add a file with the same name of one already in the project...doh.

Bye Giacomo

View solution in original post

0 Kudos
Reply
3 Replies
1,206 Views
giacomopetrini
Contributor IV

Ok, problem solved. I was trying to add a file with the same name of one already in the project...doh.

Bye Giacomo

0 Kudos
Reply
1,205 Views
CrasyCat
Specialist III

Hello

If you switched to a new Host PC, the single node license you were using till now will not work anymore on the new PC.

You need to rehost your license.

Go to www.Freescale.com then click on My Freescale. Log in into Freescale space and click on CodeWarrior Licensing.

From there you should be able to rehost your license.

CrasyCat

0 Kudos
Reply
1,205 Views
giacomopetrini
Contributor IV

I'm using the special version, so no license needed.

But the problem was another (see my other post).

Thank you anyway.

Bye Giacomo

0 Kudos
Reply