USBTAP installation problem for codewarrior version 7.0 of 568000E

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USBTAP installation problem for codewarrior version 7.0 of 568000E

Jump to solution
2,816 Views
admin
Specialist II
I need to installation codewarrior version 7 for 56800E, because to maintain our old project which transfer from our partner. this project coded by codewarrior version 7.
 
when I installed the codewarrior 7 which download from freescale website, but I can't find the USB TAP connection Item in the "Remote Connection" tap.
 
when I install the "ROHS USB TAP Update.ext",  but some problem appears. It says that:"Setup was unable to find the qulified installation of codewarrior tools on your system. Please select the location below,and press "Next" to start the file update."
 
I had choose many many different location which my codewarrior 7.0 installed, but always can't go ahead.
 
who can give me some advice to fix this USB  TAP connection for codewarrior 7.0 of 56800E.
 
Thanks
 
 
Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,282 Views
stalisman
Contributor III

Hi Xiaogang

 

I had similar problems when I installed v7.1 alongside v6.3.

 

The installations share a folder:  C:\Documents and Settings\YOUR LOGIN NAME\Local Settings\Application Data\Metrowerks.

 

This folder is updated each time you launch and IDE and it can get confused.

 

I deleted the contents of this folder and then relaunched v7.1 and the USB Tap option reappeared.

 

It is a pain that you have to redo your project settings but it worked for me.

 

 

Good luck

 

Regarding the "ROHS USB TAP Update.exe" error it's almost certainly a bug in the Update executable itself, and best ignored as clearing out the above folder will most probably solve your problem.

 

Message Edited by stalisman on 2009-07-24 11:16 AM

View solution in original post

0 Kudos
Reply
1 Reply
1,283 Views
stalisman
Contributor III

Hi Xiaogang

 

I had similar problems when I installed v7.1 alongside v6.3.

 

The installations share a folder:  C:\Documents and Settings\YOUR LOGIN NAME\Local Settings\Application Data\Metrowerks.

 

This folder is updated each time you launch and IDE and it can get confused.

 

I deleted the contents of this folder and then relaunched v7.1 and the USB Tap option reappeared.

 

It is a pain that you have to redo your project settings but it worked for me.

 

 

Good luck

 

Regarding the "ROHS USB TAP Update.exe" error it's almost certainly a bug in the Update executable itself, and best ignored as clearing out the above folder will most probably solve your problem.

 

Message Edited by stalisman on 2009-07-24 11:16 AM
0 Kudos
Reply