Software Simulation of DSC Controllers in CW IDE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Software Simulation of DSC Controllers in CW IDE

2,081件の閲覧回数
Kanthi
Contributor II

Hello Moderators,

 

    I have an interesting question. Can we do software simulation of CW IDE without using any hardware etc?

 

  I shall make it more detail: KEIL IDE supports AGSI (Advanced Graphic Simulator Interface) through which without use of external hardware or USBTAP.

Using AGSI we can create software models (which in turn perform the functionality of hardware) & interact with KEIL just a target hardware board does.

 

  Does CodeWarrior also supports any such interface? Using which we can perform Software simulation? If Yes can you please inform me.

 

 Or CW supports any other form of software simulation without using target hardware boards?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,246件の閲覧回数
Dekabrist
Contributor I

Hi

 

In the CW only MCU core simulated.

0 件の賞賛
返信