USB Tap, CCS, and Starcore 2.7.2

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

USB Tap, CCS, and Starcore 2.7.2

跳至解决方案
3,782 次查看
gtg927p
Contributor I
Hey, I have updated to Starcore DSP 2.7.2.  However, I can't seem to change the CCS from running the parallel port.  Therefore, everytime I attempt to Link in debugging, I get numerous errors.  My USB Tap is connected and flashing the green LED for TX/RX.  I think that's about all I can say about it.  Oh also, sometimes the CCS freezes when I try the config tools and does open a separate CCS when I try "config -cc usb" but it still is running the Parallel:1.
标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,091 次查看
CrasyCat
Specialist III

Hello

Can you try the following:
  - Close all CCS icon is the windows status bar.
  - Start the IDE
  - Select "File" -> "Open" and open the file {Install}\ccs\bin\ccs.cfg
  - Change "config cc Parallel:1" to "config cc utap"
  - Save the changes and close the edit window..

It should be working better.

CrasyCat

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,092 次查看
CrasyCat
Specialist III

Hello

Can you try the following:
  - Close all CCS icon is the windows status bar.
  - Start the IDE
  - Select "File" -> "Open" and open the file {Install}\ccs\bin\ccs.cfg
  - Change "config cc Parallel:1" to "config cc utap"
  - Save the changes and close the edit window..

It should be working better.

CrasyCat

0 项奖励
回复
1,091 次查看
gtg927p
Contributor I
It seems to work great now.  Thanks for the help and the very speedy response!
0 项奖励
回复