USB Tap, CCS, and Starcore 2.7.2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB Tap, CCS, and Starcore 2.7.2

Jump to solution
4,928 Views
gtg927p
Contributor I
Hey, I have updated to Starcore DSP 2.7.2.  However, I can't seem to change the CCS from running the parallel port.  Therefore, everytime I attempt to Link in debugging, I get numerous errors.  My USB Tap is connected and flashing the green LED for TX/RX.  I think that's about all I can say about it.  Oh also, sometimes the CCS freezes when I try the config tools and does open a separate CCS when I try "config -cc usb" but it still is running the Parallel:1.
Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
2,237 Views
CrasyCat
Specialist III

Hello

Can you try the following:
  - Close all CCS icon is the windows status bar.
  - Start the IDE
  - Select "File" -> "Open" and open the file {Install}\ccs\bin\ccs.cfg
  - Change "config cc Parallel:1" to "config cc utap"
  - Save the changes and close the edit window..

It should be working better.

CrasyCat

View solution in original post

0 Kudos
Reply
2 Replies
2,238 Views
CrasyCat
Specialist III

Hello

Can you try the following:
  - Close all CCS icon is the windows status bar.
  - Start the IDE
  - Select "File" -> "Open" and open the file {Install}\ccs\bin\ccs.cfg
  - Change "config cc Parallel:1" to "config cc utap"
  - Save the changes and close the edit window..

It should be working better.

CrasyCat

0 Kudos
Reply
2,237 Views
gtg927p
Contributor I
It seems to work great now.  Thanks for the help and the very speedy response!
0 Kudos
Reply