USB TAP Problem with MC56F8345

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB TAP Problem with MC56F8345

3,505件の閲覧回数
Cowboy
Contributor I
Hi
 
I just bought a USB TAP and upgrade CW to FreeScales downloadable updates to V7.3
 
In ccs with verbose on I get the following
0: USB TAP (JTAG) (utap:smileyhappy: Loader software ver. {1.6}
Sending code to USB TAP - please wait
Connection #1 accepted from localhost at Wed Oct 31 19:37:49 2007
check_min_version(serverh=0,*version)
  api version: 00000004 00000005
*** unhandled(command=4) ***
*** unhandled(command=1) ***
*** unhandled(command=0) ***
config_chain(serverh=0,cc=0,count=1,*devlist,*generic)
  devlist: hawkv2
reset_to_debug(serverh=0,cc=0)
  ERROR(5): Core not responding
Connection #1 from localhost closed at Wed Oct 31 19:37:57 2007
 
After that CW give me Core not Responding error, I've changed the JTAG speed, after installation it was 250 I increment it down to 75, and set it to 8000 and increment it down to 1000
BUT... still the same error
 
 Can any one help me please
 
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,551件の閲覧回数
J2MEJediMaster
Specialist I
For CodeWarrior for DSP 56800/E v 7.3, you need to install a RoHS patch to make later versions of the TAP work with CodeWarrior. The patch can be found on this page. Follow the link USBTAP-WIN-04-03-2006: CodeWarrior USB TAP ROHS Update (Windows) on this page to download the patch. HTH.

---Tom
0 件の賞賛
返信

1,551件の閲覧回数
Cowboy
Contributor I
Hi Tom
 
Thanks for the page but I have allready installed the update.
I can see the TAP is resetting my board but it does not whant to stay
in debug, it reatart.
 
If just update my tap in the ccs "updateutap" and it seems to be working on
my notebook but not on the PC. I'm happy with that as long as it works on the notebook.
 
Thank you
0 件の賞賛
返信

1,551件の閲覧回数
J2MEJediMaster
Specialist I
I've seen a variation on this problem and never got it sorted out. I wonder what's different between your laptop and the desktop PC?

---Tom
0 件の賞賛
返信