USB TAP Problem with MC56F8345

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB TAP Problem with MC56F8345

3,497 Views
Cowboy
Contributor I
Hi
 
I just bought a USB TAP and upgrade CW to FreeScales downloadable updates to V7.3
 
In ccs with verbose on I get the following
0: USB TAP (JTAG) (utap:smileyhappy: Loader software ver. {1.6}
Sending code to USB TAP - please wait
Connection #1 accepted from localhost at Wed Oct 31 19:37:49 2007
check_min_version(serverh=0,*version)
  api version: 00000004 00000005
*** unhandled(command=4) ***
*** unhandled(command=1) ***
*** unhandled(command=0) ***
config_chain(serverh=0,cc=0,count=1,*devlist,*generic)
  devlist: hawkv2
reset_to_debug(serverh=0,cc=0)
  ERROR(5): Core not responding
Connection #1 from localhost closed at Wed Oct 31 19:37:57 2007
 
After that CW give me Core not Responding error, I've changed the JTAG speed, after installation it was 250 I increment it down to 75, and set it to 8000 and increment it down to 1000
BUT... still the same error
 
 Can any one help me please
 
Labels (1)
0 Kudos
Reply
3 Replies

1,543 Views
J2MEJediMaster
Specialist I
For CodeWarrior for DSP 56800/E v 7.3, you need to install a RoHS patch to make later versions of the TAP work with CodeWarrior. The patch can be found on this page. Follow the link USBTAP-WIN-04-03-2006: CodeWarrior USB TAP ROHS Update (Windows) on this page to download the patch. HTH.

---Tom
0 Kudos
Reply

1,543 Views
Cowboy
Contributor I
Hi Tom
 
Thanks for the page but I have allready installed the update.
I can see the TAP is resetting my board but it does not whant to stay
in debug, it reatart.
 
If just update my tap in the ccs "updateutap" and it seems to be working on
my notebook but not on the PC. I'm happy with that as long as it works on the notebook.
 
Thank you
0 Kudos
Reply

1,543 Views
J2MEJediMaster
Specialist I
I've seen a variation on this problem and never got it sorted out. I wonder what's different between your laptop and the desktop PC?

---Tom
0 Kudos
Reply