The question with codewarrior lisense

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The question with codewarrior lisense

2,577件の閲覧回数
siufean
Contributor I

I know a lisense of codewarrior is to lock a lisense with MAC and Hardisk lable.The first question is if I want to buy such a lisense, do I need to offer my MAC&HardLable at the same time? Or, they are only needed at the register and activity moment? The second question is if my lisense machine is lost or have a hardware problem, how can I use another machine to replace the lisense one?
Hope I describe questions clear.
Thank you :smileyhappy:

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

903件の閲覧回数
Alban
Senior Contributor II
Hello,
 
When you use a license which is locked on one computer, you cannot use it on another one.
If you want a license that can be moved, you need to buy a dongle that you will be able to put on one or another computer.
The 'node' details are needed when the product is registered and the bought license issued.
 
If you plan to change your machine, it would be better to invest a bit more in the dongle.
 
Alban.
0 件の賞賛
返信

903件の閲覧回数
siufean
Contributor I
hi,
 
Thank you for your reply!
Does that mean if I lose my PC, I need to by another lisense at the same time?
0 件の賞賛
返信

903件の閲覧回数
Alban
Senior Contributor II
Yes, in principle.

After in particular cases I don't know...

Otherwise that would be far too easy!
I would say I lost my computer every month and re-sell licenses on the Internet !

There is also an option of buying floating licenses.
This way, you have a server which only gives the license when a computer uses the software.
It's a way to share a license between computers.

Alban.
0 件の賞賛
返信