Cannot set Production Target Date in download dialog

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cannot set Production Target Date in download dialog

3,947 Views
resander
Contributor I
I want to download the special edition. When I click DOWNLOAD a dialogbox pops up asking for information about project/product. I am having a problem filling in the Production Target date in this dialog.
 
When I click Calendar icon (to the right of the production target date field) another smaller dialogbox pops up that allows the user to set date. This dialog has no OK button, only a Close button at the upper right corner. When I click the Close button nothing is transferred to the production target data field. This causes Submit-form to fail.
 
How can I wriggle out of this?
 
Ken Resander
 
Labels (1)
0 Kudos
Reply
4 Replies

1,727 Views
resander
Contributor I
Many thanks. The rev 6.3 download can now be accessed..
 
The secret is to click the day in the calendar.
 
The date is set to currrent date on entry to the date dialog. I estimated time to production as about a year and just clicked 'increment year' button. I was happy with the day but did not realize I had to click the day in the calendar even though it already showed the value I wanted.
 
It would be nice:
 
 -  to have an OK button
 -  to have live display with changes reflected back on any change of year, month or day
 -  even to have plain, old, ugly, surprise-free combobox lists
 
Again many thanks.
 
Ken
 
0 Kudos
Reply

1,727 Views
J2MEJediMaster
Specialist I
When the calendar pops up for the target date, set the month and year using the GUI controls. Then click on a day in the calendar for that month, and you should be returned to the download form with the date inserted in that field. That's the behavior I got using IE6. HTH.

---Tom

0 Kudos
Reply

1,727 Views
Curt
Contributor IV
Hi resander:
It's been a while, but I made it work and I THINK I just double-clicked on a date
in the calendar.  Key data bit though is:  it will work.  (Can you expand the dialog
box?  There are a couple of places in CW where a dialog pops up with the buttons
hidden.)
 
0 Kudos
Reply

1,727 Views
Alban
Senior Contributor II
Hello Ken...

May be you could help us helping you.
We like to know which version you are working on, otherwise we cannot check most problems.

Alban.
0 Kudos
Reply