Sending Integers from 56F8347 using printf?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Sending Integers from 56F8347 using printf?

3,752件の閲覧回数
Kai
Contributor I
Hello,
 
How can i send Integers to my Computer, using the serial interface? If i use the printf funktion, the Codewarrior open an extra console. This method slows down the Controller(56F8347) and destroys my realtime for the cloosed loop control. Is there a function, which can send Integers in realtime to the serial Interface?
 
Thanks and please excuse my english



J2MEJediMaster added MCU type to header.
 
 

Message Edited by J2MEJediMaster on 2007-05-01 11:06 AM

ラベル(1)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

1,748件の閲覧回数
Alban
Senior Contributor II
Hello Kai,

There are already a lot of posts about using printf.
Please have a look at the special threads on printf and you will find your answer.

In order to do this, use the search engine at the bottom left of the page.

Cheers,
Alban.
0 件の賞賛
返信

1,748件の閲覧回数
Kai
Contributor I
Hello Alban,
 
I found nothing suitable thing searching for entries with printf. How can I switch the CONSOLE off. I would like to use the serial port and a terminal program. If the programm  uses the Console, i have nor realtime anymore.
 
Thank you
0 件の賞賛
返信

1,748件の閲覧回数
Alban
Senior Contributor II
Hello,

I think closing a component is enough for it to be switched off.

Cheers,
Alban.
0 件の賞賛
返信