Project Import

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Project Import

1,716 次查看
ankurchauhan
Contributor I

Is it possible to import CW MCU 6.4 project in to CW MCU 10.6.4.

Because when I'm trying to import ".mcp " file, Its giving tool chain error.

 

 

Regards

Ankur

标签 (1)
标记 (1)
0 项奖励
回复
2 回复数

1,557 次查看
TICS_Fiona
NXP Employee
NXP Employee

Hello Ankur

The Project Importer in v10.6 only supports DSC products.

For other products, the solution is to create a new bareboard project in CW10.6.4, and then add/copy all your source files to the new project. This is the cleanest way to import a project. Below is an application note for how to do this:

http://cache.freescale.com/files/soft_dev_tools/doc/app_note/AN4727.pdf


Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------


0 项奖励
回复

1,557 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

the file with extension .mcp is classic CW project file name.

CW10.6.4 only has CW for DSC Classic project importer, but doesn’t have other classic project importer.

With CW10.6.4, if it’s not DSC project, just follow below document to port classic CW to eclipse CW.

http://cache.freescale.com/files/soft_dev_tools/doc/app_note/AN4727.pdf?fsrch=1&sr=1&pageNum=1

does this answer your question?

Jennie

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复