Processor Expert support for M52259DEMOKIT in CodeWarrior for ColdFire V7.2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Processor Expert support for M52259DEMOKIT in CodeWarrior for ColdFire V7.2

1,703件の閲覧回数
PeteG
Contributor II

Hi

I'm using CodeWarrior for ColdFire V7.2 with a M52259DEMOKIT.

If I try to use Processor Expert or Device Initialisation I get a message saying that the M52259DEMOKIT is not supported. Is this correct and are there any updates to add this support?

 

I've noticed that the patch for CodeWarrior for ColdFire V7.1.2 adds support for this board but I can't find anything for CodeWarrior for ColdFire V7.2.

 

Thanks

ラベル(1)
0 件の賞賛
返信
1 返信

1,197件の閲覧回数
ProcessorExpert
Senior Contributor III

Hello,

 

we are sorry for inconvenience but currently there are supported only M52259EVB rev 2.0 and plain M52259 MCU in Processor Expert.

 

To use 52259DEMO, you could create a regular project for plain 52259 (not EVB) and setup the CPU bean according to DEMO PCB hardware (crystal etc..).

 

best regards
Vojtech Filip
Processor Expert Support Team

0 件の賞賛
返信